LS1046A Custom Board - MMC Error -110 MMC Tuning failed

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

LS1046A Custom Board - MMC Error -110 MMC Tuning failed

3,446 次查看
CGganesh
Contributor II

Hi,

We are facing MMC tuning error during the Linux running time in our LS1046A based custom board. Below are the error message related to the same.

####################

[ 2.047960] mmc0: Tuning timeout, falling back to fixed sampling clock
[ 2.054843] mmc0: tuning execution failed: -110
[ 2.117978] mmc0: Tuning timeout, falling back to fixed sampling clock
[ 2.124860] mmc0: tuning execution failed: -110
[ 2.187948] mmc0: Tuning timeout, falling back to fixed sampling clock
[ 2.194657] mmc0: tuning execution failed: -110
[ 2.257956] mmc0: Tuning timeout, falling back to fixed sampling clock
[ 2.264839] mmc0: tuning execution failed: -110
[ 2.327972] mmc0: Tuning timeout, falling back to fixed sampling clock
[ 2.334854] mmc0: tuning execution failed: -110
[ 2.411741] mmc0: switch to bus width 8 failed

######################

From the error we suspected that it could be because of Higher eMMC clock frequency of 150MHz. So, we tried limiting the clock frequency to 100MHz or 50MHz. Surprising the issue is evident even when the MMC is operating at 50MHz also.

We already make sure that the Voltage levels, and all timing requirements it is fine. Please let us know what can cause this failure prints,

Regards,

Ganesh

3 回复数

3,356 次查看
Hector_Villarruel
NXP TechSupport
NXP TechSupport

 

Dear CGganesh,

I have reviewed the information you have provided,
Nevertheless, I would like to ask you a few questions about this situation:

What is the type of memory you are connecting ?
Could you share more information about it ?
Is there any different change in the system on the memory part ?
Did you make any changes on the RCW ?

Best Regards,
Hector Villarruel

0 项奖励
回复

3,414 次查看
CGganesh
Contributor II

Dear NXP Team,

We are facing this issue in more number of boards now and it is stopping our development activity. Please try to provide the requested details.

Regards,

Ganesh

2,879 次查看
Ghouse
Contributor V

Hi @CGganesh 

Were u able to resolve this issue, as iam also facing the same problem, if resolved please let me know how it was resolved.

0 项奖励
回复