LS1046 power sequencing

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LS1046 power sequencing

1,423件の閲覧回数
WilfridBertrand
Contributor I

Hello,

I'm going to do the bring up of an LS1046 custom board.


The part 3.2 of the datasheet mention the following Power Sequencing :
1. OVDD, DVDD, LVDD, EVDD, TVDD, XVDD, AVDD_CGAn, AVDD_PLAT,
AVDD_D1, AVDD_SDn_PLL1, AVDD_SDn_PLL2, USB_HVDD. Drive
TA_PROG_SFP = GND.
• PORESET_B input must be driven asserted and held during this step.
2. VDD, SVDD, TA_BB_VDD, USB_SDVDD, USB_SVDD
• The 3.3 V (USB_HVDD) in Step 1 and 1.0 V (USB_SDVDD, USB_SVDD) in
Step 2 supplies can power up in any sequence provided all these USB supplies
ramp up within 95 ms with respect to each other.
3. G1VDD

Is there an issue or a risk to damage the processor if I power only the first sequence to check the power supplies signal integrity, and if I do the same for the second and third stage ?

Best regards,
Wilfrid 

タグ(2)
0 件の賞賛
返信
1 返信

1,413件の閲覧回数
Chavira
NXP TechSupport
NXP TechSupport

Hi @WilfridBertrand!

Thank you for contacting NXP Support!

If you don't follow the power sequencing you can experiment with random failures or in the worst of cases damage the processor.

If you want to check by steps but in the order, I think is not dangerous for the processor, but I can't be sure of that, we don't have documentation about that.

Best Regards

Alejandro.

0 件の賞賛
返信