LS1046 data transfer via PCIe

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LS1046 data transfer via PCIe

3,254件の閲覧回数
diljithka
Contributor I

Does LS1046 has the support data transfer via PCIe. we have a requirement for memory to pci memory and pci memory to memory t data transaction using this QDMA block in LS1046.Does LS1046 has the support for datat transfer via PCIe? can you provide the DMA driver support and sample application for the PCIe data transfer.?

0 件の賞賛
返信
3 返答(返信)

3,239件の閲覧回数
yipingwang
NXP TechSupport
NXP TechSupport

Do you use LS1046 as EP or RC device?

Please refer to the following in Linux source code.

drivers/pci/controller/dwc/pci-layerscape-ep.c

drivers/misc/pci_endpoint_test.c

Documentation/PCI/endpoint/pci-test-howto.rst

 

0 件の賞賛
返信

3,227件の閲覧回数
diljithka
Contributor I

HI @yipingwang 

thanks for your response.

we are using LS1046 as RC.

Our requirement is to transfer data via PCIe using QDMA.Is this possible in LS1046.Does the DMA engine inside LS1046 support data transfer from LS1046 to a slave device via PCIe .If so can you provide any sample application ?

 

0 件の賞賛
返信

3,215件の閲覧回数
yipingwang
NXP TechSupport
NXP TechSupport

We use the specific dmatest.c and fsl-qdma.c to test memory/PCIe DMA performance on ls1046a platform with LSDK kernel. We set PCIe address using:

echo [#pcie addr] > /sys/module/dmatest/parameters/pci_phys_addr

Please refer to Readme.txt in the attachment.

0 件の賞賛
返信