LS1046 QSPI setup time isssue at input timing

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LS1046 QSPI setup time isssue at input timing

1,677件の閲覧回数
chenjacky
Contributor I

Hi,

We found the QSPI setup time isssue at input timing. It can't meet spec.

LS1046 SDR mode QuadSPI input and output timing

Setup time for incoming data tNIIVKH 8.6 — ns
Hold time requirement for incoming data tNIIXKH 0.4 — ns

 

Our measurement result: the clock frequence is 50MHz.

QSPI_Setup_timing.bmp

At the same time, we measured at the LS1046RDB-RevB that has same issue.

But we found the clock is 70MHz, the Setup time value is 3.88 ns.

Do you have any comment?

Thanks.

2018/9/19

ラベル(1)
0 件の賞賛
返信
1 返信

1,509件の閲覧回数
andrei_skok
NXP Employee
NXP Employee

We can not guarantee LS1046A to work properly if HW specifications are violated.

You have to meet LS1046A HW specifications.

0 件の賞賛
返信