LS1046 PTP EXTTS configuration.

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LS1046 PTP EXTTS configuration.

ソリューションへジャンプ
3,004件の閲覧回数
Oleksandr1
Contributor I

I am going to use External Time Stamps for PTP timer on LS1046A CPU. Now I need to configure an input pin to be used as a TSEC1588_TRIG_IN1. According to "LS1046A Reference Manual" I need to modify the RCW[EC2] = 010. So I introduced the following change to my 'rcw' source file:

...
#include <ls1046a.rcwi>                                                 
+ EC2=2
...

Beforehand these pins controlled by RCW[EC2] (EC2_RX_DV, EC2_RXD[0], EC2_RXD[1], etc )were used to communicate with RGMII PHY and the voltage they used was 1.8v.

What voltage (3.3v or 1.8v) can I apply to TSEC1588_TRIG_IN1 pin after setting RCW[EC2] to '010' ?

Can I enable the internal pull-up resistor somehow on TSEC1588_TRIG_IN1 pin?

 

0 件の賞賛
返信
1 解決策
2,981件の閲覧回数
r8070z
NXP Employee
NXP Employee

According to the LS1046A datasheet this pin buffer powered by LVDD and LVDD can be 1.8V or 2.5V. LVDD based receivers are simple CMOS I/O circuits and satisfy appropriate LVCMOS type specifications. The datasheet Table 3 “Absolute maximum ratings for input signal voltage levels” says that Max DC V input range is GND to (LVDD x 1.1). The datasheet section “IEEE 1588 DC electrical characteristics” provides the VIH/VIL (Input high/low voltage).

The internal pull-up resistor cannot be enabled after PORESET is negation.

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
2,982件の閲覧回数
r8070z
NXP Employee
NXP Employee

According to the LS1046A datasheet this pin buffer powered by LVDD and LVDD can be 1.8V or 2.5V. LVDD based receivers are simple CMOS I/O circuits and satisfy appropriate LVCMOS type specifications. The datasheet Table 3 “Absolute maximum ratings for input signal voltage levels” says that Max DC V input range is GND to (LVDD x 1.1). The datasheet section “IEEE 1588 DC electrical characteristics” provides the VIH/VIL (Input high/low voltage).

The internal pull-up resistor cannot be enabled after PORESET is negation.

0 件の賞賛
返信