LS1043a-rdb network problem

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LS1043a-rdb network problem

Jump to solution
2,948 Views
eriktideman
Contributor III

We are using the LS1043a-rdb -pa evaluation board and having problem with ethernet in linux. When we build the kernel with the SDK-2.0's defconfig (kernel version 4.1.8) none of the ethernet interfaces RX counter increases despite connected to whatever other network equipment. TX works fine.

When switching kernel to the SDK-0.5's defconfig (kernel version 3.19) all interfaces works fine. Is there any configuration in the latest SDK that we are missing?

Labels (1)
0 Kudos
Reply
1 Solution
2,729 Views
Pavel
NXP Employee
NXP Employee

Usually similar problem happens if there is no FMAN microcode. Check your boar using the following pages:

https://freescale.sdlproducts.com/LiveContent/content/en-US/QorIQ_SDK/GUID-A83D8AAA-27F0-4E9A-BFC5-C...

https://freescale.sdlproducts.com/LiveContent/content/en-US/QorIQ_SDK/GUID-4BF3D3AB-4098-432C-820B-4...

https://freescale.sdlproducts.com/LiveContent/content/en-US/QorIQ_SDK/GUID-929B4381-1F81-4B48-B378-C...

https://freescale.sdlproducts.com/LiveContent/content/en-US/QorIQ_SDK/GUID-395614F4-A733-4219-BB1D-8...


Have a great day,
Pavel Chubakov

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
2 Replies
2,730 Views
Pavel
NXP Employee
NXP Employee

Usually similar problem happens if there is no FMAN microcode. Check your boar using the following pages:

https://freescale.sdlproducts.com/LiveContent/content/en-US/QorIQ_SDK/GUID-A83D8AAA-27F0-4E9A-BFC5-C...

https://freescale.sdlproducts.com/LiveContent/content/en-US/QorIQ_SDK/GUID-4BF3D3AB-4098-432C-820B-4...

https://freescale.sdlproducts.com/LiveContent/content/en-US/QorIQ_SDK/GUID-929B4381-1F81-4B48-B378-C...

https://freescale.sdlproducts.com/LiveContent/content/en-US/QorIQ_SDK/GUID-395614F4-A733-4219-BB1D-8...


Have a great day,
Pavel Chubakov

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply
2,729 Views
eriktideman
Contributor III

Thanks, I were not aware of this and will look at it!

Regards Erik.

0 Kudos
Reply