LS1043ARDB's SDBoot DIP switch settings with Code Warrior+JTAG

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LS1043ARDB's SDBoot DIP switch settings with Code Warrior+JTAG

Jump to solution
2,991 Views
ts1234
Contributor III

I am preparing the LS1043ARDB's development environment under CodeWarrior. I will also connect JTAG TAP.

I am unable to find LS1043ARDB's DIP Switch settings for SD Card boot  in the https://www.nxp.com/docs/en/quick-reference-guide/CWARMv8GS.pdf.

What are the recommended settings for DIP SW3, SW4 and SW5 with LS1043ARDB SD boot?

 

0 Kudos
Reply
1 Solution
2,968 Views
ufedor
NXP Employee
NXP Employee

The SDHC_SPICS controls multiplexing between SDHC_VS and SPI_CS0.

If SD card is used, then SDHC_SPICS should be 0 (OFF).

View solution in original post

3 Replies
2,980 Views
ts1234
Contributor III

What is the use of SW3[8] SDHC_SPICS switch?

What is the recommended value for CodeWarrior+JTAG setup?

 

 

0 Kudos
Reply
2,969 Views
ufedor
NXP Employee
NXP Employee

The SDHC_SPICS controls multiplexing between SDHC_VS and SPI_CS0.

If SD card is used, then SDHC_SPICS should be 0 (OFF).

2,985 Views
ufedor
NXP Employee
NXP Employee

Refer to the QorIQ LS1043A Reference Design Board Getting Started Guide, 8 DIP switches:

https://www.nxp.com/webapp/Download?colCode=LS1043ARDBGSG&location=null

0 Kudos
Reply