LS1043ARDB-PA/PB evaluation board.

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LS1043ARDB-PA/PB evaluation board.

ソリューションへジャンプ
2,417件の閲覧回数
trondwang
Contributor I

Hi,

in the schematic diagram of the evaluation board there is a power U46 that creates a voltage (S1VDD_SRC) that not seems to be connected.

What is the reason for this power?

thanks and regards,

Trond Inge#

ラベル(1)
タグ(2)
0 件の賞賛
返信
1 解決策
2,105件の閲覧回数
r8070z
NXP Employee
NXP Employee

Have a great day,

Some revisions of the LS1043ARDB-PA have the LS1043A S1VDD powered from the U46.

S1VDD_SRC.png

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
2,106件の閲覧回数
r8070z
NXP Employee
NXP Employee

Have a great day,

Some revisions of the LS1043ARDB-PA have the LS1043A S1VDD powered from the U46.

S1VDD_SRC.png

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信