LS1043AQDS: QSPI

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

LS1043AQDS: QSPI

2,854 次查看
carlos-m-ribeiro
Contributor I

Hello,

Can you help us about the reference/manufacturer of the QSPI that you used during the tests with LS1043AQDS u-boot?

Best regards

0 项奖励
回复
6 回复数

2,847 次查看
carlos-m-ribeiro
Contributor I

And would you know if these QSPI flashes are also compatible with LS1043AQDS: Winbond W25Q256JWEIQ and Macronix MX25L25635FZ2I-10G?

Thank you again

0 项奖励
回复

2,844 次查看
ufedor
NXP Employee
NXP Employee

QSPI controller of the LS1043A has flexible sequence engine to support various flash vendor devices.

0 项奖励
回复

2,840 次查看
carlos-m-ribeiro
Contributor I
And you have any idea what can be wrong in our tests: using the QSPI flash MX25L25635FZ2I-10G and write the RCW file rcw_1600_qspiboot.bin.swapped from packages/firmware/rcw/ls1043aqds/RR_FQPP_1455/ in address 0x0, and u-boot.bin/u-boot-dtb.bin (generated using ls1043aqds_qspi_defconfig) in address 0x100000 we could not seen any output/print in our board.
 
Best regards
0 项奖励
回复

2,834 次查看
carlos-m-ribeiro
Contributor I
Using ls1043aqds in our board we can not seen any CPU accesses to QSPI, and we guaranty that bootstraps are correctly. What we should do to view CPU accesses to QSPI.
 
Thank you.
0 项奖励
回复

2,821 次查看
ufedor
NXP Employee
NXP Employee

It is required to doublecheck the processor connection schematics referring the Design Checklist and evaluation board design files.

Also check that TRST_B is pulsed low (asserted) during POR sequence.

0 项奖励
回复

2,850 次查看
ufedor
NXP Employee
NXP Employee

S25FL128SAGMFIR0 on a riser card was used.

0 项奖励
回复