LS1043AQDS: QSPI

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LS1043AQDS: QSPI

2,859件の閲覧回数
carlos-m-ribeiro
Contributor I

Hello,

Can you help us about the reference/manufacturer of the QSPI that you used during the tests with LS1043AQDS u-boot?

Best regards

0 件の賞賛
返信
6 返答(返信)

2,852件の閲覧回数
carlos-m-ribeiro
Contributor I

And would you know if these QSPI flashes are also compatible with LS1043AQDS: Winbond W25Q256JWEIQ and Macronix MX25L25635FZ2I-10G?

Thank you again

0 件の賞賛
返信

2,849件の閲覧回数
ufedor
NXP Employee
NXP Employee

QSPI controller of the LS1043A has flexible sequence engine to support various flash vendor devices.

0 件の賞賛
返信

2,845件の閲覧回数
carlos-m-ribeiro
Contributor I
And you have any idea what can be wrong in our tests: using the QSPI flash MX25L25635FZ2I-10G and write the RCW file rcw_1600_qspiboot.bin.swapped from packages/firmware/rcw/ls1043aqds/RR_FQPP_1455/ in address 0x0, and u-boot.bin/u-boot-dtb.bin (generated using ls1043aqds_qspi_defconfig) in address 0x100000 we could not seen any output/print in our board.
 
Best regards
0 件の賞賛
返信

2,839件の閲覧回数
carlos-m-ribeiro
Contributor I
Using ls1043aqds in our board we can not seen any CPU accesses to QSPI, and we guaranty that bootstraps are correctly. What we should do to view CPU accesses to QSPI.
 
Thank you.
0 件の賞賛
返信

2,826件の閲覧回数
ufedor
NXP Employee
NXP Employee

It is required to doublecheck the processor connection schematics referring the Design Checklist and evaluation board design files.

Also check that TRST_B is pulsed low (asserted) during POR sequence.

0 件の賞賛
返信

2,855件の閲覧回数
ufedor
NXP Employee
NXP Employee

S25FL128SAGMFIR0 on a riser card was used.

0 件の賞賛
返信