LS1043A gerber data

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LS1043A gerber data

2,669 Views
jindrichbrett
Contributor II

Hello guys,

have you got somebody cad data for LS1043A in version 23x23 780pin bga.

Or at least some excel table where the pins are digestelly described in some order please.

It is too complicated in pdf, because for example 1 pin is in 5 tables...

Thank you very much

Jindrich

Labels (1)
0 Kudos
Reply
2 Replies

2,533 Views
r8070z
NXP Employee
NXP Employee

Have a great day,

You can create a technical case with request for a LS1043A reference board gerber files. See How I could create a Service Request?

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

2,533 Views
jindrichbrett
Contributor II

Hi Serguei,

thanks a lot.

Jindrich

0 Kudos
Reply