LS1043A gerber data

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LS1043A gerber data

2,658件の閲覧回数
jindrichbrett
Contributor II

Hello guys,

have you got somebody cad data for LS1043A in version 23x23 780pin bga.

Or at least some excel table where the pins are digestelly described in some order please.

It is too complicated in pdf, because for example 1 pin is in 5 tables...

Thank you very much

Jindrich

ラベル(1)
0 件の賞賛
返信
2 返答(返信)

2,522件の閲覧回数
r8070z
NXP Employee
NXP Employee

Have a great day,

You can create a technical case with request for a LS1043A reference board gerber files. See How I could create a Service Request?

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

2,522件の閲覧回数
jindrichbrett
Contributor II

Hi Serguei,

thanks a lot.

Jindrich

0 件の賞賛
返信