LS1043A cfg_rcw_src setting for NAND Flash

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LS1043A cfg_rcw_src setting for NAND Flash

2,240件の閲覧回数
ajaykumar_d
Contributor II

Hi I am using LS1043A in my project and want to boot from NAND flash of size 8Gb(1GB). The cfg_rcw_src supported for NAND flash is 4k page and 128 pages/block but the NANDs avilable from Micron and tosiba supports only 4K page and 64pages/block. Is it possible to put some customised cfg_rcw_src setting for 4k page and 64pages/block.

ラベル(1)
タグ(1)
0 件の賞賛
返信
2 返答(返信)

2,007件の閲覧回数
ajaykumar_d
Contributor II

hi, I tried this option and is working fine for me. thanks a lot for your advice.

0 件の賞賛
返信

2,007件の閲覧回数
ufedor
NXP Employee
NXP Employee

It is possible to use cfg_rcw_src=1_0001_xxxx (8-bit NAND Flash, 4 KB page, 128 pages/block), in U-Boot it is required to specify correct block size - 64 pages.