LS1043A as network switch using OpenWRT

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LS1043A as network switch using OpenWRT

Jump to solution
3,182 Views
carljones
Contributor III

Hello NXP,

I connected VSC8531 and VSC8575 PHYs to an LS1043A chip to create a 6-port media server running on OpenWRT. I tried to configure one port as WAN and the rest of the ports as 5-port switch. Did you have a guide on how to achieve this? Currently, each port is configured independently, as if an individual network card on a PC.

Kind regards,

Carlos

Tags (2)
0 Kudos
Reply
1 Solution
3,165 Views
bpe
NXP Employee
NXP Employee

There is no dedicated support in LSDK to L2 bridging for processors equipped
with DPAA1. You can use the kernel L2 bridge, which is a pure software
implementation and should work with any generic Ethernet interface driver.
Details on the kernel native Ethernet bridge can be found at this link.
For hardware-accelerated bridging, consider moving to a DPAA2 processor,
LS1088, LS2088, LX2160 and their derivatives.

Best Regards,
Platon

 

View solution in original post

0 Kudos
Reply
2 Replies
3,166 Views
bpe
NXP Employee
NXP Employee

There is no dedicated support in LSDK to L2 bridging for processors equipped
with DPAA1. You can use the kernel L2 bridge, which is a pure software
implementation and should work with any generic Ethernet interface driver.
Details on the kernel native Ethernet bridge can be found at this link.
For hardware-accelerated bridging, consider moving to a DPAA2 processor,
LS1088, LS2088, LX2160 and their derivatives.

Best Regards,
Platon

 

0 Kudos
Reply
2,839 Views
carljones
Contributor III

Hi @bpe Platon,

Haven't really thanked you on this.

Thank you very much.

Regards

 

0 Kudos
Reply