LS1043A as network switch using OpenWRT

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LS1043A as network switch using OpenWRT

ソリューションへジャンプ
3,200件の閲覧回数
carljones
Contributor III

Hello NXP,

I connected VSC8531 and VSC8575 PHYs to an LS1043A chip to create a 6-port media server running on OpenWRT. I tried to configure one port as WAN and the rest of the ports as 5-port switch. Did you have a guide on how to achieve this? Currently, each port is configured independently, as if an individual network card on a PC.

Kind regards,

Carlos

タグ(2)
0 件の賞賛
返信
1 解決策
3,183件の閲覧回数
bpe
NXP Employee
NXP Employee

There is no dedicated support in LSDK to L2 bridging for processors equipped
with DPAA1. You can use the kernel L2 bridge, which is a pure software
implementation and should work with any generic Ethernet interface driver.
Details on the kernel native Ethernet bridge can be found at this link.
For hardware-accelerated bridging, consider moving to a DPAA2 processor,
LS1088, LS2088, LX2160 and their derivatives.

Best Regards,
Platon

 

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
3,184件の閲覧回数
bpe
NXP Employee
NXP Employee

There is no dedicated support in LSDK to L2 bridging for processors equipped
with DPAA1. You can use the kernel L2 bridge, which is a pure software
implementation and should work with any generic Ethernet interface driver.
Details on the kernel native Ethernet bridge can be found at this link.
For hardware-accelerated bridging, consider moving to a DPAA2 processor,
LS1088, LS2088, LX2160 and their derivatives.

Best Regards,
Platon

 

0 件の賞賛
返信
2,857件の閲覧回数
carljones
Contributor III

Hi @bpe Platon,

Haven't really thanked you on this.

Thank you very much.

Regards

 

0 件の賞賛
返信