LS1043A-RGW boot failure

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LS1043A-RGW boot failure

4,214 Views
tmorrison
Contributor III

We have a custom board - largely based upon the NXP LS1043A-RGW Development board

We are using the LSDK 18.03 with some patches to be able to customize it. We are having

some problems in several different areas, but I have patched around those to try to get linux

to boot all the way.

The LSDK is flex-builder based and I have built a firmware,  bootpartition, and rootfs. I load

that onto a sd card, and try to boot from that SD Card. I get this at the end:

[    3.411691] EXT4-fs (mmcblk0p3): couldn't mount as ext3 due to feature incompatibilities
[    3.453190] EXT4-fs (mmcblk0p3): mounted filesystem with ordered data mode. Opts: (null)
[    3.461292] VFS: Mounted root (ext4 filesystem) on device 179:3.
[    3.468133] devtmpfs: error mounting -2
[    3.472210] Freeing unused kernel memory: 832K
[    3.476726] Kernel panic - not syncing: No working init found.  Try passing init= option to kernel. See Linux Documentation/admin-guide/init.rst for guidance.
[    3.490883] CPU: 1 PID: 1 Comm: swapper/0 Not tainted 4.14.16-dirty #6
[    3.497397] Hardware name: LS1043A RGW Board (DT)
[    3.502089] Call trace:
[    3.504531] [<ffff000008088c70>] dump_backtrace+0x0/0x370
[    3.509920] [<ffff000008088ff4>] show_stack+0x14/0x20
[    3.514963] [<ffff000008b0e380>] dump_stack+0x9c/0xbc
[    3.520004] [<ffff0000080c7b18>] panic+0x11c/0x28c
[    3.524785] [<ffff000008b2093c>] kernel_init+0xec/0x100
[    3.529999] [<ffff000008084be0>] ret_from_fork+0x10/0x18
[    3.535301] SMP: stopping secondary CPUs
[    3.539215] Kernel Offset: disabled
[    3.542692] CPU features: 0x002004
[    3.546082] Memory Limit: none
[    3.549129] ---[ end Kernel panic - not syncing: No working init found.  Try passing init= option to kernel. See Linux Documentation/admin-guide/init.rst for guidance.

I am assuming that the lsdk shouldn't have any of the problems that Linux Documentation/admin-guide/init.rst

Labels (1)
0 Kudos
Reply
7 Replies

4,015 Views
tmorrison
Contributor III

can you please answer my questions I have asked about

0 Kudos
Reply

4,015 Views
bpe
NXP Employee
NXP Employee

Your recent inputs are not quite inline with the oirginal problem description. I particular, you are running fsck over /dev/sdd4 which should be a HDD based on it's name, but the problem is,  according to what you wrote earlier,  with a bootable SD card. fsck can help, but only if used in the proper way: if you can boot your system with a tinydistro ramdisk, try mounting the problematic partition by hand and running fsck on the target.

Regards,

Platon

0 Kudos
Reply

4,015 Views
tmorrison
Contributor III

I will try this test soon!

0 Kudos
Reply

4,015 Views
bpe
NXP Employee
NXP Employee

Your Linux cannot mount the root filesystem due to certain FS feature
incompatibility. It is important how you format your SD card partitions
to put the images created by flex-builder. Use flex-installer from the
same LSDK release to populate your boot SD card. If you prefer to
format it by hand, look at flex-installer code, procedure partition_format_storage_device()
for the mkfs.ext4  invocation options. Note that you are
working with a pretty much obsolete LSDK version. You need to use
Ubuntu 16.04 on your build host for everything to work smoothly. Also, if it
is a heavily customized kernel, compare the LSDK default kernel configuration
with your one to ensure all necessary filesystem support options are
enabled.

Please keep in mind, that we can provide a very limited support to
historical (l)SDK releases. If the suggestions above do not help,
our recommendation is to move to the most recent LSDK.


Have a great day,
Platon

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply

4,015 Views
tmorrison
Contributor III

Hi Platon,

Thank you for your quick response.

I am using the flex-installer that came with this LSDK.

I am sorry that this was NOT clear.

I will look at hand formatting.

I am using Ubuntu 18.04 because that was required for some of

the other LSDKs that I've unsuccessfully had no luck getting it to

work with a LS1043A-RGW.

I am not sure how to "downgrade" my Ubuntu to support this?

In addition, I am using this version of the LSDK because I was given

patches from you guys (NXP/Freescale) that explicitly patch this version

of LSDK to support the LS1043A-RGW BSP. There are no supported

patches for newer LSDK's - I certainly would use them if I could.

I will update after I try hand formatting.

Tom

0 Kudos
Reply

4,015 Views
tmorrison
Contributor III

Hi,

I compared the flex-installer for the newest SDK with this - and there was one parameter I added.

Still no luck....

I have a couple more questions about this:

It says here that it successfully mounted it:

  [    3.637912] EXT4-fs (mmcblk0p3): couldn't mount as ext3 due to feature incompatibilities
  [    3.673534] EXT4-fs (mmcblk0p3): mounted filesystem with ordered data mode. Opts: (null)
  [    3.681636] VFS: Mounted root (ext4 filesystem) on device 179:3.

Why it is trying to mount as ext3 first, I also did an e2fsck on this partition:

  tom@newSNIPC:~$ sudo e2fsck /dev/sdd4
  e2fsck 1.44.1 (24-Mar-2018)
  system: clean, 71311/1479856 files, 645570/5912960 blocks

So, I am confused why it is having an issue. There is a /sbin/init (points to /lib/systemd/systemd)

Thanks in advance.

Tom

0 Kudos
Reply

4,015 Views
tmorrison
Contributor III

I don't think this is answered completely - still not working for me - and I have verified everything I can.

0 Kudos
Reply