LS1043A PBL SD Card Boot

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LS1043A PBL SD Card Boot

ソリューションへジャンプ
2,434件の閲覧回数
vbonduro
Contributor II

Hello,

Section 27.5 of the QorIQ LS1043A Reference Manual, Rev. 3, 02/2017 States the following:

The PBL starts searching for the first good block. It begins to fetch the PBL image at the
starting address of that block.

Few questions on these two statements:

1. What represents a "good block"? (eg. a well formatted RCW?)

2. What is the definition of a PBL Image? (eg. Is it the RCW + PBI commands, just the RCW, etc. ?)

3. Does the PBL search for the RCW or must it exist at the starting address (for SD Card, sector 8)?

Thanks

ラベル(1)
タグ(3)
1 解決策
2,174件の閲覧回数
bpe
NXP Employee
NXP Employee


 Q1 and Q3: The Manual is not very accurate. Actually, it performs
 no search,  just reads the card sector 8, "good" means  readable.
 
 Q2: See LS1043ARM, Section 27.4.3

Have a great day,
Platon

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

1 返信
2,175件の閲覧回数
bpe
NXP Employee
NXP Employee


 Q1 and Q3: The Manual is not very accurate. Actually, it performs
 no search,  just reads the card sector 8, "good" means  readable.
 
 Q2: See LS1043ARM, Section 27.4.3

Have a great day,
Platon

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------