LS1043A Linux SDK and yocto

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LS1043A Linux SDK and yocto

Jump to solution
4,487 Views
Naveenkumar_Muthusamy
Contributor IV

Hi,

 

we are using LS1043A in our application, we are trying to setup the build environment, we would like to know about the build options available, for ex yocto build or SDK availble for this processor, where we can customize it accordding to the board we have.

kindly provide details regarding the yocto or linux build systems and other tools which can be used for development using this ls1043a processor

0 Kudos
Reply
1 Solution
4,418 Views
yipingwang
NXP TechSupport
NXP TechSupport

RT Patch is not provided in the above release.

Please check whether the following Real-Time Edge Yocto release is what you need.

https://www.nxp.com/design/design-center/software/development-software/real-time-edge-software:REALT...

View solution in original post

0 Kudos
Reply
9 Replies
4,464 Views
yipingwang
NXP TechSupport
NXP TechSupport

If you want to use Ubuntu filesystem, you need to use "Layerscape Linux Distribution POC" release, please refer to section "3.5.2 Download Yocto bitbake" in https://www.nxp.com.cn/docs/en/user-guide/UG10081_LLDP_6.1.55_2.2.0.pdf  to download the Yocto build environment.

$ repo init -u https://github.com/nxp-qoriq/yocto-sdk -b mickledore -m ls-6.1.55-2.2.0_distro.xml

$ repo sync

$ source ./distro-setup-env -m ls1043ardb

 

If you only want to use the normal Yocto generated rootfs filesystem, you could download Yocto build environment from the following link.

https://github.com/nxp-qoriq/yocto-sdk

The latest version is YP 5.2-lf-6.12.20.

0 Kudos
Reply
4,462 Views
Naveenkumar_Muthusamy
Contributor IV

Hi @yipingwang ,

Thanks for your reply,

what is the laytest linux kernel version used in layerscape SDK. i have seen the document you have shared and it is mentioned Kernel v6.1.55. is this is the latest?

we are using pCie in our system as a root complex, does ls1043 running layerscape yocto with Kernel v6.1.55 should be okay to communicate with an FPGA running as Pcie endpoint?

 

will there be any difficulties? or challenges?

 

LS1043A

0 Kudos
Reply
4,459 Views
yipingwang
NXP TechSupport
NXP TechSupport

If you want to use Ubuntu filesystem, the latest Linux Kernel version is 6.1.55.

It is OK to use Kernel 6.1.55 to implement your purpose.

0 Kudos
Reply
4,427 Views
Naveenkumar_Muthusamy
Contributor IV

Hi @yipingwang,

thanks for the reply.

Do we have RT Patch available for the linux in the yocto you have suggested?

 

LS1043A 

0 Kudos
Reply
4,419 Views
yipingwang
NXP TechSupport
NXP TechSupport

RT Patch is not provided in the above release.

Please check whether the following Real-Time Edge Yocto release is what you need.

https://www.nxp.com/design/design-center/software/development-software/real-time-edge-software:REALT...

0 Kudos
Reply
4,314 Views
Naveenkumar_Muthusamy
Contributor IV

Hi @yipingwang ,

 

Thanks for your reply.

How to use DMA for the Pcie transfer? using DMA for PCIe interface will subsequently use DDR3/DDR4 which in turn improves performance of PCIE?

 

How the LS1043A can be Programmed ?

using JTAG?

what is the purpose of JTAG, since there is no controller core in ls1043a

or just create a wic image and write into SD and boot?

 

is it possible to use JTAG to Transfer image to ls1043a?

 

 

 

0 Kudos
Reply
4,309 Views
Naveenkumar_Muthusamy
Contributor IV
0 Kudos
Reply
4,311 Views
yipingwang
NXP TechSupport
NXP TechSupport

Please address your new questions in a new thread.

0 Kudos
Reply
4,467 Views
Naveenkumar_Muthusamy
Contributor IV

hi all,

any update on this ?

0 Kudos
Reply