LS1043A - I2C module registers accessibility issue

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LS1043A - I2C module registers accessibility issue

2,221件の閲覧回数
babatejbotcha
Contributor I

I want to enable I2C1 module(INA220A) in LS1043A board. From reference manual of LS1043A, I2C module registers are accessible in supervisor mode only. Code warrior hello world project is setting up in EL3. So, i have changed the exceptionl level to EL1(supervisor mode) from EL3 and trying to access the I2C module registers. But, getting an synchronous exception and the reason is shown up in ESR_EL1 register as "Data Abort taken without a change in Exception level" even Pstate current exception value is 4(EL1). PFA for Exception register snapshot. Please let me know why we are getting exception even while accessing I2C registers in EL1 mode. Note: Even we tried in accessing EL2, EL3, still the result is same.

ラベル(1)
タグ(1)
0 件の賞賛
返信
1 返信

2,051件の閲覧回数
Pavel
NXP Employee
NXP Employee

Look at the Section 8.3.4.3 of NXP SDK 2.0-1703 documentation:

https://www.nxp.com/docs/en/supporting-information/QORIQ-SDK-2.0-IC-REV0.pdf

 

This Section contains description for using the INA220 Linux driver.

 

See also the Section 8.4.1.

 

See the Chapter 11.4 of NXP LSDK 18.03 documentation about using the INA220 Linux driver:

https://www.nxp.com/docs/en/supporting-information/LSDK-KC-REV18.03.pdf


Have a great day,
Pavel Chubakov

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信