LS1043A, GPIO Query

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

LS1043A, GPIO Query

3,009 次查看
logeshs
Contributor II

Hi,

In LS1043A, GPIO muxed signals really confusing me a lot. At earlier stage of design i shared a Muxed signals list which i'm going to use in my system NXP engineers verified it and said MUX selction is correct. But later when i asked the similar doubt whether SPI remaining chip select pins can be used as GPIO, they said we cannot use it as GPIO. 

My First query on MUX signals in below link,

LS1043A MUX SIGNAL SELECTION 

query on SPI Chip select in below link,

https://community.nxp.com/thread/446454 

Kindly if you provide me the document or any support with List of available GPIOs (remaining GPIOs) in LS1043A when particular interfaces are used. so that we can design accordingly. 

Thanks.

标签 (1)
标记 (1)
0 项奖励
回复
3 回复数

2,631 次查看
alexander_yakov
NXP Employee
NXP Employee

To verify pin multiplexing, we offer Pinmux tool. This tool is a part of our CodeWarrior ARM v8 software.

CodeWarrior ARMv8 64 bit|NXP 


Have a great day,
Alexander

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复

2,631 次查看
logeshs
Contributor II

Hi,


Thanks for your help.
I have downloaded the tool, but could not identify where it is. Could you please help me where to find the Pin Mux inside CoreWarrior?

Could you give me the path?

Thanks

0 项奖励
回复

2,631 次查看
alexander_yakov
NXP Employee
NXP Employee

1. Please run "CodeWarrior for ARMv8"

2. Please create new "QorIQ Configuration Project" selecting necessary processor and enabling "Pin Muxing Configuration"

3. Please see "PinMux1" component in components window.

0 项奖励
回复