LS1043A Debug APB Slave Address Map

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LS1043A Debug APB Slave Address Map

5,147 Views
Xiemens
Contributor I

HI, I had found Address Map for APB-AP mapped debug modules in Table 79-5. of  S32V234RM.pdf https://www.nxp.com.cn/webapp/Download?colCode=S32V234RM&docLang=en 

But I can't found Address Map for APB-AP mapped debug modules in LS1043ARM.pdf   https://www.nxp.com.cn/webapp/Download?colCode=LS1043ARM&lang_cd=zh 

Where I can get it?

BR.

0 Kudos
Reply
6 Replies

5,114 Views
yipingwang
NXP TechSupport
NXP TechSupport

Please refer to "Appendix C EPU register descriptions" in LS1043ARM.

0 Kudos
Reply

5,099 Views
Xiemens
Contributor I

@yipingwang 

Thanks to reply.

The "Appendix C EPU register descriptions" mentioned Event Processor Debug Reservation Register n (EPRSRV0 - EPRSRV7) , Is it similar to Table 79-5. of  S32V234RM?

Debug APB Component         System Address

Cortex-A53A ROM Table         0x40089000  
Cortex-A53 A0 Debug              0x4008A000
Cortex-A53 A0 CTI                   0x40089000

For a = 0 to 7:

($DCSR_BASE + $EPU_BASE + EPRSRVa) = 0x07_0000_0000 + 0x6_0000 +
FECh + (a × -4h) = 0x07_0006_0FECh +(a × -4h)  

Cortex-A53 A0 Debug              7_0006_0FECh +(0 × -4h)
Cortex-A53 A0 CTI                  7_0006_0FECh + (1 × -4h)

Cortex-A53 A1 Debug              7_0006_0FECh +(2 × -4h)
Cortex-A53 A1 CTI                  7_0006_0FECh + (3 × -4h)

Is that correct ??

BR

 

 

0 Kudos
Reply

5,085 Views
yipingwang
NXP TechSupport
NXP TechSupport

I will discuss with the AE team, will provide more update later.

5,057 Views
Xiemens
Contributor I

@yipingwang  Hi,What about the Latest progress of Debug Adress Map?

I have another question about CodeWarrior TAP support for Eclipse IDE and where can I get the reference document?

0 Kudos
Reply

4,926 Views
yipingwang
NXP TechSupport
NXP TechSupport

Please refer to the following update from the AE team.

The LS1043A does not have an APB AP module in it.

0 Kudos
Reply

5,017 Views
yipingwang
NXP TechSupport
NXP TechSupport

For CodeWarrior TAP, you need to install the latest CodeWarrior for ARMv8 11.5.12.

The attached is CodeWarrior for ARMv8 user manual.

0 Kudos
Reply