LS1043A DPAA work queue strict-only scheduling in a channel

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LS1043A DPAA work queue strict-only scheduling in a channel

ソリューションへジャンプ
2,557件の閲覧回数
cyrilstrejc
Contributor III

In LS1043A DPAA hardware, current work queue (WQ) scheduling follows two level scheduler schema, which is mixture of strict and round-robin prioritization.

wx-prioritization.png

Is somehow possible to simplify the DPAA approach and use only 8 strict priorities with round robin completely disabled? (WQ 0 -> Priority 0, WQ 1 -> Priority 1, WQ 2 -> Priority 2, ..., WQ 7 -> Priority 7. Higher priority WQ has absolute strict priority over all lower priority WQs)

ラベル(1)
タグ(1)
0 件の賞賛
返信
1 解決策
2,427件の閲覧回数
alexander_yakov
NXP Employee
NXP Employee

It is not possible to use 8 strict priorities. In other words, it's not possible to disable round robin selection that is used for medium and low priority tiers.


Have a great day,
Alexander
TIC

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

1 返信
2,428件の閲覧回数
alexander_yakov
NXP Employee
NXP Employee

It is not possible to use 8 strict priorities. In other words, it's not possible to disable round robin selection that is used for medium and low priority tiers.


Have a great day,
Alexander
TIC

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------