LS1043A DO-254 Support

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LS1043A DO-254 Support

1,973件の閲覧回数
avionicsAndries
Contributor I

I found a technology whitepaper from Curtiss Wright (Is Arm the Future for Airborne Platforms in Military and Aerospace?) that makes the following statement in relation to a DO-254 certified project done with the NXP LS1043A:

"NXP provides documentation from the processor’s design, development and manufacturing stages that allows board manufacturers to demonstrate adherence to DO-254 requirements without the complex and time-consuming undertaking of conducting these internal tests themselves."

I previously found EUF-SNT-T1469, that provides a high-level overview of NXP's process in Avionics/Defense applications, but not nearly enough details to build a certification case. I'm interested to get more information about the level of documentation and support NXP is willing to provide from the design, development and manufacturing stages that would allow board manufacturers to demonstrate adherence without having to conduct some internal tests. 

タグ(1)
0 件の賞賛
返信
1 返信

1,533件の閲覧回数
AvionicsMat
Contributor I

I would also be interested in Certification precedence for these cores

0 件の賞賛
返信