LS1043A DDR4 configuration problem

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LS1043A DDR4 configuration problem

1,648 Views
jack_huang1
Contributor IV

At present, the configuration of DDR4 is 2GB on the reference design of ls1043a-rdb. What changes should be made to the hardware and software to support the 16GB DDR4? Thank you very much!

Labels (1)
Tags (1)
0 Kudos
Reply
1 Reply

1,587 Views
ufedor
NXP Employee
NXP Employee

The LS1043ARDB DDR settings are provided in the "u-boot/board/freescale/ls1043ardb/ddr.c":

u-boot/ddr.h at integration · qoriq-open-source/u-boot · GitHub

structure "ddr_raw_timing".

> What changes should be made to the hardware and software to support the 16GB DDR4?

It could depend on the specific SDRAM implementation.

0 Kudos
Reply