LS1043A DDR4 configuration problem

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LS1043A DDR4 configuration problem

1,614件の閲覧回数
jack_huang1
Contributor IV

At present, the configuration of DDR4 is 2GB on the reference design of ls1043a-rdb. What changes should be made to the hardware and software to support the 16GB DDR4? Thank you very much!

ラベル(1)
タグ(1)
0 件の賞賛
返信
1 返信

1,553件の閲覧回数
ufedor
NXP Employee
NXP Employee

The LS1043ARDB DDR settings are provided in the "u-boot/board/freescale/ls1043ardb/ddr.c":

u-boot/ddr.h at integration · qoriq-open-source/u-boot · GitHub

structure "ddr_raw_timing".

> What changes should be made to the hardware and software to support the 16GB DDR4?

It could depend on the specific SDRAM implementation.

0 件の賞賛
返信