LS1043 watchdog clock source

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LS1043 watchdog clock source

1,501 Views
sedat_altun
Contributor III

 

Is it possible to make the watchdog functional on an LS1043-based custom board without an RTC clock input?

Can we set another internal clock source as the input to watchdog?

Thanks in advance

Tags (1)
0 Kudos
Reply
2 Replies

1,491 Views
Oswalag
NXP TechSupport
NXP TechSupport

Hello,

Unfortunately, it is not possible.

The RTC functionality is clarified in the LS1043A Design Checklist, Table 42. Clock pin termination checklist:
"RTC is the only clock source for WDOG functionality."

 

Regards.

0 Kudos
Reply

1,307 Views
sedat_altun
Contributor III

Thank you very much 

0 Kudos
Reply