LS1043 run vpp problem, clib_elf_parse_file: open `linux-vdso.so.1': No such file or directory

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LS1043 run vpp problem, clib_elf_parse_file: open `linux-vdso.so.1': No such file or directory

4,087 Views
lixiaofan
Contributor II

Hi Guys & yipingwang‌

I can setup l2fwd dpdk sample, next step I want to use vpp, according LSDK-KC-REV18.12.pdf 9.3.4, for LS1046 and LS1043 Board setup,

then start up vpp,

#/usr/local/bin/vpp heapsize 200M unix { nodaemon } or

#/usr/local/bin/vpp heapsize 200M unix { interactive }

occur errors, tart up vpp

#/usr/local/bin/vpp heapsize 200M

seems no error, is this caused by memsize?

My mem config info:

root@localhost:~# cat /proc/sys/vm/nr_hugepages
128

root@localhost:~# cat /proc/cmdline
console=ttyS0,115200 ... default_hugepagesz=2MB hugepagesz=2MB hugepages=128 isolcpus=1 bportals=s0 qportals=s0 iommu.passthrough=1

Any reply will be very appreciated, thanks!

vpp log info:
root@localhost:~# /usr/local/bin/vpp heapsize 200M unix { nodaemon }
vlib_plugin_early_init:361: plugin path /usr/local/lib/vpp_plugins
load_one_plugin:189: Loaded plugin: abf_plugin.so (ACL based Forwarding)
load_one_plugin:189: Loaded plugin: acl_plugin.so (Access Control Lists)
load_one_plugin:189: Loaded plugin: avf_plugin.so (Intel Adaptive Virtual Function (AVF) Device Plugin)
load_one_plugin:191: Loaded plugin: cdp_plugin.so
load_one_plugin:189: Loaded plugin: dpdk_plugin.so (Data Plane Development Kit (DPDK))
load_one_plugin:189: Loaded plugin: flowprobe_plugin.so (Flow per Packet)
load_one_plugin:189: Loaded plugin: gbp_plugin.so (Group Based Policy)
load_one_plugin:189: Loaded plugin: gtpu_plugin.so (GTPv1-U)
load_one_plugin:189: Loaded plugin: igmp_plugin.so (IGMP messaging)
load_one_plugin:189: Loaded plugin: ila_plugin.so (Identifier-locator addressing for IPv6)
load_one_plugin:189: Loaded plugin: ioam_plugin.so (Inbound OAM)
load_one_plugin:117: Plugin disabled (default): ixge_plugin.so
load_one_plugin:189: Loaded plugin: l2e_plugin.so (L2 Emulation)
load_one_plugin:189: Loaded plugin: lacp_plugin.so (Link Aggregation Control Protocol)
load_one_plugin:189: Loaded plugin: lb_plugin.so (Load Balancer)
load_one_plugin:189: Loaded plugin: mactime_plugin.so (Time-based MAC source-address filter)
load_one_plugin:189: Loaded plugin: map_plugin.so (Mapping of address and port (MAP))
load_one_plugin:189: Loaded plugin: memif_plugin.so (Packet Memory Interface (experimental))
load_one_plugin:189: Loaded plugin: nat_plugin.so (Network Address Translation)
load_one_plugin:189: Loaded plugin: nsh_plugin.so (Network Service Header)
load_one_plugin:189: Loaded plugin: nsim_plugin.so (network delay simulator plugin)
load_one_plugin:117: Plugin disabled (default): perfmon_plugin.so
load_one_plugin:189: Loaded plugin: pppoe_plugin.so (PPPoE)
load_one_plugin:189: Loaded plugin: srv6ad_plugin.so (Dynamic SRv6 proxy)
load_one_plugin:189: Loaded plugin: srv6am_plugin.so (Masquerading SRv6 proxy)
load_one_plugin:189: Loaded plugin: srv6as_plugin.so (Static SRv6 proxy)
load_one_plugin:189: Loaded plugin: stn_plugin.so (VPP Steals the NIC for Container integration)
load_one_plugin:189: Loaded plugin: svs_plugin.so (Source VRF Select)
load_one_plugin:189: Loaded plugin: tlsopenssl_plugin.so (openssl based TLS Engine)
load_one_plugin:117: Plugin disabled (default): unittest_plugin.so
load_one_plugin:189: Loaded plugin: vmxnet3_plugin.so (VMWare Vmxnet3 Device Plugin)
/usr/local/bin/vpp[3086]: clib_elf_parse_file: open `linux-vdso.so.1': No such file or directory
/usr/local/bin/vpp[3086]: received signal SIGSEGV, PC unsupported, faulting address 0x80000
Aborted
root@localhost:~# /usr/local/bin/vpp heapsize 200M unix { interactive }
vlib_plugin_early_init:361: plugin path /usr/local/lib/vpp_plugins
load_one_plugin:189: Loaded plugin: abf_plugin.so (ACL based Forwarding)
load_one_plugin:189: Loaded plugin: acl_plugin.so (Access Control Lists)
load_one_plugin:189: Loaded plugin: avf_plugin.so (Intel Adaptive Virtual Function (AVF) Device Plugin)
load_one_plugin:191: Loaded plugin: cdp_plugin.so
load_one_plugin:189: Loaded plugin: dpdk_plugin.so (Data Plane Development Kit (DPDK))
load_one_plugin:189: Loaded plugin: flowprobe_plugin.so (Flow per Packet)
load_one_plugin:189: Loaded plugin: gbp_plugin.so (Group Based Policy)
load_one_plugin:189: Loaded plugin: gtpu_plugin.so (GTPv1-U)
load_one_plugin:189: Loaded plugin: igmp_plugin.so (IGMP messaging)
load_one_plugin:189: Loaded plugin: ila_plugin.so (Identifier-locator addressing for IPv6)
load_one_plugin:189: Loaded plugin: ioam_plugin.so (Inbound OAM)
load_one_plugin:117: Plugin disabled (default): ixge_plugin.so
load_one_plugin:189: Loaded plugin: l2e_plugin.so (L2 Emulation)
load_one_plugin:189: Loaded plugin: lacp_plugin.so (Link Aggregation Control Protocol)
load_one_plugin:189: Loaded plugin: lb_plugin.so (Load Balancer)
load_one_plugin:189: Loaded plugin: mactime_plugin.so (Time-based MAC source-address filter)
load_one_plugin:189: Loaded plugin: map_plugin.so (Mapping of address and port (MAP))
load_one_plugin:189: Loaded plugin: memif_plugin.so (Packet Memory Interface (experimental))
load_one_plugin:189: Loaded plugin: nat_plugin.so (Network Address Translation)
load_one_plugin:189: Loaded plugin: nsh_plugin.so (Network Service Header)
load_one_plugin:189: Loaded plugin: nsim_plugin.so (network delay simulator plugin)
load_one_plugin:117: Plugin disabled (default): perfmon_plugin.so
load_one_plugin:189: Loaded plugin: pppoe_plugin.so (PPPoE)
load_one_plugin:189: Loaded plugin: srv6ad_plugin.so (Dynamic SRv6 proxy)
load_one_plugin:189: Loaded plugin: srv6am_plugin.so (Masquerading SRv6 proxy)
load_one_plugin:189: Loaded plugin: srv6as_plugin.so (Static SRv6 proxy)
load_one_plugin:189: Loaded plugin: stn_plugin.so (VPP Steals the NIC for Container integration)
load_one_plugin:189: Loaded plugin: svs_plugin.so (Source VRF Select)
load_one_plugin:189: Loaded plugin: tlsopenssl_plugin.so (openssl based TLS Engine)
load_one_plugin:117: Plugin disabled (default): unittest_plugin.so
load_one_plugin:189: Loaded plugin: vmxnet3_plugin.so (VMWare Vmxnet3 Device Plugin)
clib_elf_parse_file: open `linux-vdso.so.1': No such file or directory
Aborted

 

root@localhost:~# /usr/local/bin/vpp heapsize 200M
vlib_plugin_early_init:361: plugin path /usr/local/lib/vpp_plugins
load_one_plugin:189: Loaded plugin: abf_plugin.so (ACL based Forwarding)
load_one_plugin:189: Loaded plugin: acl_plugin.so (Access Control Lists)
load_one_plugin:189: Loaded plugin: avf_plugin.so (Intel Adaptive Virtual Function (AVF) Device Plugin)
load_one_plugin:191: Loaded plugin: cdp_plugin.so
load_one_plugin:189: Loaded plugin: dpdk_plugin.so (Data Plane Development Kit (DPDK))
load_one_plugin:189: Loaded plugin: flowprobe_plugin.so (Flow per Packet)
load_one_plugin:189: Loaded plugin: gbp_plugin.so (Group Based Policy)
load_one_plugin:189: Loaded plugin: gtpu_plugin.so (GTPv1-U)
load_one_plugin:189: Loaded plugin: igmp_plugin.so (IGMP messaging)
load_one_plugin:189: Loaded plugin: ila_plugin.so (Identifier-locator addressing for IPv6)
load_one_plugin:189: Loaded plugin: ioam_plugin.so (Inbound OAM)
load_one_plugin:117: Plugin disabled (default): ixge_plugin.so
load_one_plugin:189: Loaded plugin: l2e_plugin.so (L2 Emulation)
load_one_plugin:189: Loaded plugin: lacp_plugin.so (Link Aggregation Control Protocol)
load_one_plugin:189: Loaded plugin: lb_plugin.so (Load Balancer)
load_one_plugin:189: Loaded plugin: mactime_plugin.so (Time-based MAC source-address filter)
load_one_plugin:189: Loaded plugin: map_plugin.so (Mapping of address and port (MAP))
load_one_plugin:189: Loaded plugin: memif_plugin.so (Packet Memory Interface (experimental))
load_one_plugin:189: Loaded plugin: nat_plugin.so (Network Address Translation)
load_one_plugin:189: Loaded plugin: nsh_plugin.so (Network Service Header)
load_one_plugin:189: Loaded plugin: nsim_plugin.so (network delay simulator plugin)
load_one_plugin:117: Plugin disabled (default): perfmon_plugin.so
load_one_plugin:189: Loaded plugin: pppoe_plugin.so (PPPoE)
load_one_plugin:189: Loaded plugin: srv6ad_plugin.so (Dynamic SRv6 proxy)
load_one_plugin:189: Loaded plugin: srv6am_plugin.so (Masquerading SRv6 proxy)
load_one_plugin:189: Loaded plugin: srv6as_plugin.so (Static SRv6 proxy)
load_one_plugin:189: Loaded plugin: stn_plugin.so (VPP Steals the NIC for Container integration)
load_one_plugin:189: Loaded plugin: svs_plugin.so (Source VRF Select)
load_one_plugin:189: Loaded plugin: tlsopenssl_plugin.so (openssl based TLS Engine)
load_one_plugin:117: Plugin disabled (default): unittest_plugin.so
load_one_plugin:189: Loaded plugin: vmxnet3_plugin.so (VMWare Vmxnet3 Device Plugin)

Labels (2)
Tags (1)
0 Kudos
Reply
1 Reply

3,635 Views
yipingwang
NXP TechSupport
NXP TechSupport

Please refer to the attached VPP setting up procedure in the attached log provided by the testing team.

Please refer to the following bootargs

root=/dev/sda4 rw rootdelay=10 console=ttyS0,115200 earlycon=uart8250,mmio,0x21c0500 ramdisk_size=0x40000000 bportals=s0 qportals=s0 isolcpus=1-3 mem=3072M default_hugepagesz=2m hugepagesz=2m hugepages=448 nmi_watchdog=0 rcupdate.rcu_cpu_stall_suppress=1

The following error could be ignored.

vpp[4610]: clib_elf_parse_file: open `linux-vdso.so.1': No such file or directory

Please refer to the following procedure to build vpp into rootfs.

1. source setup.env

2. CONFIG_APP_VPP=y in configs/build_lsdk.cfg

3. $ flex-builder -c vpp

    $ flex-builder -i merge-component

 

Thanks,

Yiping

0 Kudos
Reply