LS1043 SFP interface on SGMII

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LS1043 SFP interface on SGMII

2,151 Views
EbyJayan88
Contributor I

We are having design progressing With LS1043. There are 4 Ethernet Interfaces planned , 2 Copper and 2 Fiber (SFP). Copper Ports will be Interfaced via RGMII to EC1 and EC2 . Planning to Use Serdes Lane A and Lane B as SGMII mode to connect the SFP . Can I connect the SFP directly to the SGMII. Is there any Retimers required ? Is there any timing or Electrical Compatibility issue .

EbyJayan88_0-1619807326128.pngEbyJayan88_0-1619807326128.png

 

 

0 Kudos
Reply
2 Replies

2,025 Views
EbyJayan88
Contributor I

Can you share part number for SPF recommended to be used with LS1043

0 Kudos
Reply

2,147 Views
ufedor
NXP Employee
NXP Employee

> Can I connect the SFP directly to the SGMII.

It is possible if SFP with SGMII interface is used.

0 Kudos
Reply