LS1043 SFP interface on SGMII

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LS1043 SFP interface on SGMII

2,153件の閲覧回数
EbyJayan88
Contributor I

We are having design progressing With LS1043. There are 4 Ethernet Interfaces planned , 2 Copper and 2 Fiber (SFP). Copper Ports will be Interfaced via RGMII to EC1 and EC2 . Planning to Use Serdes Lane A and Lane B as SGMII mode to connect the SFP . Can I connect the SFP directly to the SGMII. Is there any Retimers required ? Is there any timing or Electrical Compatibility issue .

EbyJayan88_0-1619807326128.pngEbyJayan88_0-1619807326128.png

 

 

0 件の賞賛
返信
2 返答(返信)

2,027件の閲覧回数
EbyJayan88
Contributor I

Can you share part number for SPF recommended to be used with LS1043

0 件の賞賛
返信

2,149件の閲覧回数
ufedor
NXP Employee
NXP Employee

> Can I connect the SFP directly to the SGMII.

It is possible if SFP with SGMII interface is used.

0 件の賞賛
返信