LS1043 Hreset

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LS1043 Hreset

3,107 Views
crazy210
Contributor I

LS1043 reset circuit:

The connection relationship is shown in the figure:

one PMIC,model is MC34VR500VAES.

one FPGA,model is xc7a15tcsg324.

one LS1043,model is LS1043AXE7QQB.

one power-on reset chip U3,model is ADM8611N293ACBZ-R7.

two input and gate U1, U2, model is 74LVC1G08.

one OCTAL BUFFERS/DRIVERS WITH 3-STATE OUTPUTS U4,model is SN74LVCH244APW.

 

crazy210_0-1681288480514.png

 

crazy210_1-1681288480607.png

 

The follow is a detailed description of the circuit:

The pin 1 of U1 is connected to the power-on status output of PMIC, it indicates that the PMIC is powered on. The pin 2 of U1 are disconnected during operation.

U3 is a 200ms power-on reset, the output of U1 and the output of U3 output a reset through U2 AND gate, which is connected to pin 2 and pin 4 of U4 as inputs. Pin 18 and pin 16 of U4 are output pins, respectively are connected to FPGA, LS1043. HRRESET_B_18 and PORESET_B_18, which are all pulled up to 1.8v.  

Why is HRESET_B_18 only 700Mv? See the yellow waveform below, the blue waveform is PORESET_B_18, and the waveform is 1.8V, What is the reason?

 

crazy210_2-1681288482533.png

 

0 Kudos
Reply
1 Reply

3,043 Views
yipingwang
NXP TechSupport
NXP TechSupport

Please refer to section "4.3 Power-on reset recommendations" in the attached application note.

0 Kudos
Reply