LS1043 DDR4 single chip support

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LS1043 DDR4 single chip support

2,054 Views
Ajesh_Cam01
Contributor I

Is it possible use LS1043A with single chip 16bit DDR4?

0 Kudos
Reply
3 Replies

2,034 Views
Ajesh_Cam01
Contributor I

 Thanks for the reply...Is there any errata available for LS1043A. I am not able to find from product page.

0 Kudos
Reply

2,032 Views
ufedor
NXP Employee
NXP Employee

Errata is a confidential document available only under NDA. Please create a Technical Case using your corporate email to request the NDA signing. 

0 Kudos
Reply

2,048 Views
ufedor
NXP Employee
NXP Employee

It is possible - refer to the QorIQ LS1043A Reference Manual, 18.2 DDR Features:

• Data bus widths supported:
• 32-/36-bit
• 16-/20-bit

"/" - means with ECC.