LS1043 DDR4 single chip support

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LS1043 DDR4 single chip support

2,053件の閲覧回数
Ajesh_Cam01
Contributor I

Is it possible use LS1043A with single chip 16bit DDR4?

0 件の賞賛
返信
3 返答(返信)

2,033件の閲覧回数
Ajesh_Cam01
Contributor I

 Thanks for the reply...Is there any errata available for LS1043A. I am not able to find from product page.

0 件の賞賛
返信

2,031件の閲覧回数
ufedor
NXP Employee
NXP Employee

Errata is a confidential document available only under NDA. Please create a Technical Case using your corporate email to request the NDA signing. 

0 件の賞賛
返信

2,047件の閲覧回数
ufedor
NXP Employee
NXP Employee

It is possible - refer to the QorIQ LS1043A Reference Manual, 18.2 DDR Features:

• Data bus widths supported:
• 32-/36-bit
• 16-/20-bit

"/" - means with ECC.