LS1028a reset fuses to '0' in development mode?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LS1028a reset fuses to '0' in development mode?

916件の閲覧回数
mbourhis
Contributor II

Hi,

I am currently working on the SecureBoot for my board.

During the step of 'development' or 'testing',

is there a way to reset or set to '0' the SRKH fuses, after they have been blown

by the command 'mw 0x01e80020 0x2' (write '0x2' in the SFP_INGR register).

 

Or maybe, is there a way to 'test' the SecureBoot without blow the SRHK fuses?

 

Thank you for your help.

Best regards,

 

Mikael Bourhis

タグ(1)
0 件の賞賛
返信
1 返信

906件の閲覧回数
ufedor
NXP Employee
NXP Employee

> is there a way to reset or set to '0' the SRKH fuses, after they have been blown

There is no such way.

> is there a way to 'test' the SecureBoot without blow the SRHK fuses?

Please refer to the Layerscape Software Development Kit User Guide, 6.1.1.5.2.4.1 Program SRKH mirror registers in CodeWarrior environment, 4. Platform LS1028A (TA 3.x).

 

0 件の賞賛
返信