LS1028a reset fuses to '0' in development mode?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LS1028a reset fuses to '0' in development mode?

908 Views
mbourhis
Contributor II

Hi,

I am currently working on the SecureBoot for my board.

During the step of 'development' or 'testing',

is there a way to reset or set to '0' the SRKH fuses, after they have been blown

by the command 'mw 0x01e80020 0x2' (write '0x2' in the SFP_INGR register).

 

Or maybe, is there a way to 'test' the SecureBoot without blow the SRHK fuses?

 

Thank you for your help.

Best regards,

 

Mikael Bourhis

Tags (1)
0 Kudos
Reply
1 Reply

898 Views
ufedor
NXP Employee
NXP Employee

> is there a way to reset or set to '0' the SRKH fuses, after they have been blown

There is no such way.

> is there a way to 'test' the SecureBoot without blow the SRHK fuses?

Please refer to the Layerscape Software Development Kit User Guide, 6.1.1.5.2.4.1 Program SRKH mirror registers in CodeWarrior environment, 4. Platform LS1028A (TA 3.x).

 

0 Kudos
Reply