LS1028ARDB no bootable Linux Kernel from git repo?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LS1028ARDB no bootable Linux Kernel from git repo?

1,690件の閲覧回数
jens_neumann
Contributor I

Hey,

I've been trying for over a week now to install an Ubuntu Distro on the LS1028ARDB via SD-Card. I am doing everything according to manual, but it appears that simply cloning the qoriq repo yields an unusable Kernel version, as it doesn't contain the drivers necessary to use the ethernet interfaces. Switching to LS1028a-early-access branch did help a bit, as in I managed to launch Ubuntu, but then the bridge interface can't be configured properly. So the question is: Is there a pre-built image to use with Ubuntu (which would be ideal)? Or can you at least tell me which Git branch is guaranteed to work NOW with the current Ubuntu userland etc.?

If you force your customers to build everything themselves, then please at least ensure that everything works not only on release of the manual (it appears the most recent one is from April), but also today.

0 件の賞賛
返信
1 返信

1,595件の閲覧回数
Pavel
NXP Employee
NXP Employee

Build image for your board using the following command:

flex-builder -i mkfw -m ls1028ardb -b sd

 

Find .img file using the following path:

/flexbuild/build/images/firmware_ls1028ardb_uboot_sdboot.img

 

Connect SD card using SD card reader to your PC host.

Write this image to SD on your PC host using the following command

sudo dd if= firmware_ls1028ardb_uboot_sdboot.img of=/dev/sdb bs=512 seek=8

Have a great day,
Pavel Chubakov

 

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信