LS1028ARDB CodeWarrior TAP connects but will not return Connection Diagnostics

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LS1028ARDB CodeWarrior TAP connects but will not return Connection Diagnostics

2,936件の閲覧回数
JBKauffman
Contributor I

Hi Everyone,

I'm using an LS1028AARB development board and can connect using a TAP connected via USB and step through bare board samples like the hello_world.c  so the TAP is clearly working.   I am not however able to get the "Connection Diagnostics" to run.   It starts and will go for hours without returning any results.   How do I go about debugging this?

The only change I have made is to the configuration to set "USE_SAFE_RCW = True"

Here is a screen shot of CodeWarrior connected and stepping through the hello_world.c bare machine example:

 

JBKauffman_0-1693243358634.png

 

But when I disconnect and try running Diagnose Connection - or if I start from scratch and run diagnose connection I get the same results - it hangs with the progress bar going on for hours without showing any test being run - here is a screen shot:

 

JBKauffman_1-1693243696959.png

 

Looking at the error log I do see a stack overflow - perhaps related?   

!ENTRY org.eclipse.ui 4 0 2023-08-28 13:23:50.623
!MESSAGE Unhandled event loop exception
!STACK 0
java.lang.StackOverflowError
	at org.eclipse.swt.internal.win32.OS.CallWindowProc(Native Method)
...

Maybe related I'm also not able to bring up the CCS command window - if I navigate to:

C:\Freescale\CW4NET_v2020.06\Common\CCS\bin>ccs.exe

It just returns without any errors but I don't have the CCS icon in the IDE unless I am missing it someplace.

Looking for advice.

 

Thanks!

 

Jeff

0 件の賞賛
返信
6 返答(返信)

2,869件の閲覧回数
SebastianG
NXP TechSupport
NXP TechSupport

Hello @JBKauffman,

In order to verify that everything is set as expected, could you please tell me the steps that you use to run the bareboard project in Codewarrior?

Regards,

Sebastian

0 件の賞賛
返信

2,847件の閲覧回数
JBKauffman
Contributor I

Hi Sebastian,

After installing CodeWarrior and applying the latest update (as shown above) I did the following:

1. From Window->show view->other->Target Connections Duplicated the LS1028A RDB configuration and performed the probe discovery to connect my TAP via USB

2. Edited the target initialization and changed USE_SAFE_RCW = False to USE_SAFE_RCW = True

3. Created a new project: File->new->codewarrior_stationary and selected a bare board project:

JBKauffman_0-1693580704944.png

4. Run->debug configurations and can step through the code run etc... everything works as expected

5. Try to do a Diagnose Connection as shown before and it never returns anything

 

 

0 件の賞賛
返信

2,763件の閲覧回数
SebastianG
NXP TechSupport
NXP TechSupport

Hi @JBKauffman,

Apologies for the delayed response,

In order to avoid any kind of confusion:

Could you please provide your Codewarrior version?

Could you please provide your Tap Codewarrior  version?

Could you please provide your Codewarrior TAP Firmware boot loader version? (Please see in the reference the attached log from Tera Term)

0 件の賞賛
返信

2,818件の閲覧回数
SebastianG
NXP TechSupport
NXP TechSupport

Hello @JBKauffman,

I would like to inform you that I keep working to replicate your last reply from my side.

I would let you know as soon as I have an update.

Thank you so much for patience

Regards,

Sebastian

0 件の賞賛
返信

2,882件の閲覧回数
SebastianG
NXP TechSupport
NXP TechSupport

hello @JBKauffman,

I would like to inform you that I'm working on your question, I will let you know as soon as I have an update.

Thank you so much for your patience

Regards,

Sebastian

0 件の賞賛
返信

2,933件の閲覧回数
JBKauffman
Contributor I

Forgot to include the version:

JBKauffman_0-1693245759678.png

 

0 件の賞賛
返信