LS1028A switch port configuration problem

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LS1028A switch port configuration problem

1,169 Views
hqq2312
Contributor I

Hello,

I need some help to configure the switch port(swp0-3).

Question 1:

Only about a few seconds the board will print the information shown below when I open it, but I don't get the reason.

[ 283.739793] mscc_felix 0000:00:00.5 swp2: failed (err=-2) to del object (id=3)
[ 283.747151] mscc_felix 0000:00:00.5 swp1: failed (err=-2) to del object (id=3 )
[ 283.754979] mscc_felix 0000:00:00.5 swp0: failed (err=-2) to del object (id=3 )
[ 283.762490] mscc_felix 0000:00:00.5 swp2: failed (err=-2) to del object (id=3 )
[ 283.769967] mscc_felix 0000:00:00.5 swp1: failed (err=-2) to del object (id=3 )
[ 283.777419] mscc_felix 0000:00:00.5 swp0: failed (err=-2) to del object (id=3 )

Question 2:

When I want to configure switch device interfaces for swp0, swp1, swp2 and swp3 acrroding to the Real-time Edge Software User Guide, I always get the following reply.

hqq2312_2-1709626904887.png

 ls /sys/bus/pci/devices/0000:00:00.5/net/
swp0 swp1 swp2 swp3
 ip link add name switch type bridge vlan_filtering 1
 ip link set switch up
 ip link set swp0 master switch && ip link set swp0 up
RTNETLINK answers: No such device
 ip link set swp0 master switch
RTNETLINK answers: No such device

Please tell me how to figure these two questions, thank you!

 

Labels (2)
0 Kudos
Reply
0 Replies