LS1028A RDB USB interface

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LS1028A RDB USB interface

1,788件の閲覧回数
mkraj
Contributor III

Dear Expert

We are doing USB interface modifications of LS1028A RDB by connecting both usb3.0 interfaces to the M.2 connecctors for connecting 4g modem and we are not using any USB connector.

we are not using below usb interface pins

1. R_USB1_VBUS- not using

2. USB1_ID -connecting to ground with 1K

3.USB_DRVVBUS-not using

4.USB_PWRFAULT-not using

5.USB2_VBUS-not using

6. USB2_ID-connecting to ground with 1K

 

Is it ok? Please comment.

 

Thank you in advance

With Regards

Krishnam Raju M

0 件の賞賛
返信
1 返信

1,759件の閲覧回数
mrudangshelat-13
NXP TechSupport
NXP TechSupport

Hi @mkraj,

Please refer to Table 32 in the AN12028 for pin termination details if the USB interface is unused.

Regards,
Mrudang