LS1028A RDB USB interface

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

LS1028A RDB USB interface

1,869 次查看
mkraj
Contributor III

Dear Expert

We are doing USB interface modifications of LS1028A RDB by connecting both usb3.0 interfaces to the M.2 connecctors for connecting 4g modem and we are not using any USB connector.

we are not using below usb interface pins

1. R_USB1_VBUS- not using

2. USB1_ID -connecting to ground with 1K

3.USB_DRVVBUS-not using

4.USB_PWRFAULT-not using

5.USB2_VBUS-not using

6. USB2_ID-connecting to ground with 1K

 

Is it ok? Please comment.

 

Thank you in advance

With Regards

Krishnam Raju M

0 项奖励
回复
1 回复

1,840 次查看
mrudangshelat-13
NXP TechSupport
NXP TechSupport

Hi @mkraj,

Please refer to Table 32 in the AN12028 for pin termination details if the USB interface is unused.

Regards,
Mrudang