LS1028 : l2switch: ping fail

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LS1028 : l2switch: ping fail

1,759件の閲覧回数
bharat_chaudhar
Contributor II

Hi, 

I'm trying a setup as provided in the " 4.2.12.3.3.3.2 CPU port without bridge"

remote-host(192.168.3.2) -----connected-to---- swp3(192.168.3.1) 

I've used the script as provided in the section

ping from remote-host to ip 192.168.3.1 is failing.

 

Please provide inputs on how to proceed

Thanks,

Bharat 

 

0 件の賞賛
返信
1 返信

1,753件の閲覧回数
yipingwang
NXP TechSupport
NXP TechSupport

I assume that you are using LSDK 2004 Linux Kernel 5.4.

Please refer to the attached script for switch configuration without bridge.

root@ls1028ardb:~# bash +x enetc_switch_cpu_port_without_bridge_dsa.sh

root@ls1028ardb:~# ifconfig swp3 down
root@ls1028ardb:~# echo $?
0
root@ls1028ardb:~# ifconfig swp3 100.1.1.29 netmask 255.255.255.0
[ 90.042476] mscc_felix 0000:00:00.5 swp3: configuring for inband/qsgmii link mode
[ 90.050569] 8021q: adding VLAN 0 to HW filter on device swp3
root@ls1028ardb:~# echo $?
0
root@ls1028ardb:~# [ 93.131335] mscc_felix 0000:00:00.5 swp3: Link is Up - 1Gbps/Full - flow control off
[ 93.139218] IPv6: ADDRCONF(NETDEV_CHANGE): swp3: link becomes ready
ifconfig swp0 up
root@ls1028ardb:~# echo $?
0
root@ls1028ardb:~# ping -c 5 -s 1 100.1.1.1

0 件の賞賛
返信