LS1028 FSPI device driver not work

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LS1028 FSPI device driver not work

1,494件の閲覧回数
zhicheng1
Contributor III

Hi  

I want to use qspi feature of the ls1028 processer.  I change the dts as below:

dts:

spi@20c0000 {
compatible = "nxp,lx2160a-fspi";
#address-cells = <0x01>;
#size-cells = <0x00>;
reg = <0x00 0x20c0000 0x00 0x10000 0x00 0x20000000 0x00 0x10000000>;
reg-names = "fspi_base\0fspi_mmap";
interrupts = <0x00 0x19 0x04>;
clocks = <0x02 0x02 0x00 0x02 0x02 0x00>;
clock-names = "fspi_en\0fspi";
status = "okay";
phandle = <0x30>;
qspidevice@0 {
compatible = "nxp,qspi-generic";
#address-cells = <0x01>;
#size-cells = <0x01>;
spi-max-frequency = <0x1312d00>;
reg = <0x00>;
spi-rx-bus-width = <0x04>;
spi-tx-bus-width = <0x01>;
phandle = <0x31>;
};
/*
flash@0 {
compatible = "spansion,m25p80";
#address-cells = <0x01>;
#size-cells = <0x01>;
m25p,fast-read;
spi-max-frequency = <0x1312d00>;
reg = <0x00>;
spi-rx-bus-width = <0x04>;
spi-tx-bus-width = <0x01>;
phandle = <0x31>;
};
*/
};

 

Can I use "spi_sync" API to wirte the qspi device driver code as fallow? if not , which api should be called?

some driver code: 
static ssize_t qspi_write(struct file *file, const char __user *buf, size_t count, loff_t *ppos)
{
    struct qspi_dev *qspi = file->private_data;
    char write_buf[256];
    size_t len = min(count, sizeof(write_buf));
    struct spi_transfer xfer;
    struct spi_message msg;
    int ret;

    if (copy_from_user(write_buf, buf, len)) {
        dev_err(qspi->dev, "Failed to copy data from user space\n");
        return -EFAULT;
    }

    printk(KERN_INFO "  write_buf: %s\n",write_buf);
    dump_spi_device(qspi->spi);
    memset(&xfer, 0, sizeof(xfer));
    xfer.tx_buf = write_buf;
    xfer.rx_buf = NULL;
    xfer.len = len;
    //xfer.cs_change = 1;
    //xfer.bits_per_word = qspi->spi->bits_per_word;
    //xfer.speed_hz = qspi->spi->max_speed_hz;

    spi_message_init(&msg);
    spi_message_add_tail(&xfer, &msg);

    ret = spi_sync(qspi->spi, &msg);
    if (ret < 0) {
        dev_err(qspi->dev, "Failed to write to QSPI, error code: %d\n", ret);
        //dev_err(qspi->dev, "Message length: %u, Message buffer: %p\n", msg.len, msg.buf);
        return ret;
    }
 
Thanks,
zhang
0 件の賞賛
返信
2 返答(返信)

1,489件の閲覧回数
mikelooijmans
Contributor IV

Most QSPI controllers can only be used in combination with flash memories (serial NOR typically, some also support serial NAND). They cannot handle "generic" SPI as they "snoop" the commands sent to control the extra data lines.

Connect your device to a "normal" SPI controller (the NXP has plenty of those).

0 件の賞賛
返信

1,473件の閲覧回数
zhicheng1
Contributor III

get it.

Thanks.

0 件の賞賛
返信