LS1026A PCIE not completing reset

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LS1026A PCIE not completing reset

3,137件の閲覧回数
renaud
Contributor IV

We have a ls1026A design with the RCW set as follows:

0e0d0012 10000000 00000000 00000000

33338888 40a05012 40025000 c1000000

00000000 00000000 00000000 0003dbb8

20124000 01003100 00000096 00000001

The PCIe is defined by 8888 as PCIe4x, our connection to the device  is Gen2.

We do not get link as the reset sequence is not completing as shown by the PLL1RSTCTL register.

What could hold the PCIe bus like that?

 

ラベル(1)
0 件の賞賛
返信
5 返答(返信)

2,979件の閲覧回数
renaud
Contributor IV

e seem to have an intermittent problem. The connected PCIE device only appears 60% of the time.

0 件の賞賛
返信

3,112件の閲覧回数
renaud
Contributor IV
Line two of RCW has been replaced by:
00008888 00e05012 40025000 c1000000
0 件の賞賛
返信

3,086件の閲覧回数
yipingwang
NXP TechSupport
NXP TechSupport

Investigating this problem, will update later.

0 件の賞賛
返信

3,042件の閲覧回数
renaud
Contributor IV

We switched to use SRDS protocol 5559 and it worked with one PCIe lane. That is all we need but if you find an answer I am interested to know.

0 件の賞賛
返信

3,121件の閲覧回数
renaud
Contributor IV

Actually, the title of my request is not descriptive enough.

We have an issue with the PLL clock not locking on SD2. 100Mz clock input is there though.

0 件の賞賛
返信