LS1026, DDR4 validation, read SPD data lost

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LS1026, DDR4 validation, read SPD data lost

4,545件の閲覧回数
rudolfusselmann
Contributor II

Hello,

we have a custom board with an LS1046A and a DDR4 DIMM module.

I have extensively read the QCVS_DDR_User_Guide.pdf.


When I start QCVS and create a new QorIQ DDR validation project, I have the option to read the SPD. After I read the SPD, I get the green check mark. I go ahead and click FINISH.

Now when I go to the Component Explorer, and look at the DDR properties, I click on "SPD Data" and then on the "..."  Now, I expect to see the SPD data, but it is not populated (I get two empty boxes).  I do see a file "ddr_spd.properties" in the project folder, and when I open it, it appears to contain the SPD data in XML format. Lots and lots data in that file ...

I have followed all the steps as outlined in QCVS_DDR_User_Guide section 1.1.4.1, pages 22-25, but do not get the same behavior. 

 

I am running Ubuntu 22.04, in case that matters.

 

Any pointers appreciated !

 

Many Thanks,

rudi

タグ(4)
0 件の賞賛
返信
4 返答(返信)

4,499件の閲覧回数
rudolfusselmann
Contributor II

Thank you for your message Yiping !

I am following these same steps as you are in your picture, but I do not understand how to make the SPD data move up.

Please see my attachment.

Many Thanks !

rudi

0 件の賞賛
返信

4,463件の閲覧回数
yipingwang
NXP TechSupport
NXP TechSupport

Please check whether you can continue to do validation in QCVS DDRv tool.

0 件の賞賛
返信

4,457件の閲覧回数
rudolfusselmann
Contributor II

 

Yes, I can continue, and we do get optimal settings. 

 

I am wondering why the tool does not work for me as it supposed to ?

0 件の賞賛
返信

4,508件の閲覧回数
yipingwang
NXP TechSupport
NXP TechSupport

Please refer to my following screenshot captured when connecting CodeWarrior to LS1046ARDB.

yipingwang_0-1706522046214.png

Do you have LS1046ARDB? If yes, please connect your CodeWarrior to LS1046ARDB to do verification.

0 件の賞賛
返信