LS1021a- Custom Board - NAND Chip not detected under Linux

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

LS1021a- Custom Board - NAND Chip not detected under Linux

2,562 次查看
sanjuvarghese
Contributor II

Hi,

I am facing a NAND issue under Linux. The NAND chip is working under u-boot as I can Erase/Read/Write the chip. But Linux is unable to load the NAND driver successfully. The mtd/nand/fsl_ifc_nand.c always failing in this condition

if (!fsl_ifc_ctrl_dev || !fsl_ifc_ctrl_dev->regs)

       return -ENODEV;

I checked the the driver for fsl_ifc_ctrl_dev and it is getting updated in memory/fsl/ifc.c probe function(fsl_ifc_ctrl_probe). But the Linux is not calling the probe function. If I am manually allocating the memory of fsl_ifc_ctrl_dev in fsl_ifc_nand.c by adding the following lines

fsl_ifc_ctrl_dev = kzalloc(sizeof(*fsl_ifc_ctrl_dev), GFP_KERNEL);

  if (!fsl_ifc_ctrl_dev)

  return -ENOMEM;

Now the error moved to this location

ret = of_address_to_resource(node, 0, &res);

  if (ret) {

  dev_err(&dev->dev, "%s: failed to get resource\n", __func__);

  return ret;

  }

Here is my device tree settings

ls1021a.dtsi:

-------------

ifc: ifc@1530000 {

                        compatible = "fsl,ifc","simple-bus";

                        reg = <0x0 0x1530000 0x0 0x10000>;

                        interrupts = <GIC_SPI 75 IRQ_TYPE_LEVEL_HIGH>;

}

ls1021aiot.dts :

----------------

&ifc {

        #address-cells = <2>;

        #size-cells = <1>;

        ranges = <0x0 0x0 0x7e800000 0x10000>;

        status = "okay";

        nand@0{                                

                #address-cells = <1>;

                #size-cells = <1>;

                compatible = "fsl,ifc-nand";

                reg = <0x0 0 0x10000>;

                bank-width = <1>;

                device-width = <1>;

        };

Can you please help us to solve the NAND issue in linux?

Thanks In advance

Sanju

标签 (1)
0 项奖励
回复
2 回复数

2,243 次查看
scottwood
NXP Employee
NXP Employee

The memory/fsl/ifc.c driver is required.  You can't replace it with a struct full of zeroes.  You need to determine why it is not getting probed.  What board/SoC is this?  If a custom board, what do your dts and board C files look like?

0 项奖励
回复

2,243 次查看
Pavel
NXP Employee
NXP Employee

Usually Linux kernel does not change IFC initialization for the NAND.

Test NAND Flash operations under u-boot.

What messages do you see for the NAND using under Linux?


Have a great day,
Pavel

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复