LS1021ATWR : Sata Command Not Found In U-boot

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

LS1021ATWR : Sata Command Not Found In U-boot

跳至解决方案
8,703 次查看
vigneshr
Contributor III

Hi All,

I was trying use sata interface in ls1021atwr board for sdk 1.7, but it is showing sata command not found. Could someone help me how to enable/add the sata command in u-boot ?

Is there any macros should be added or any patch to be applied ?

Here is the u-boot log,

U-Boot 2014.07+ls1+g659b6a2 (Jun 09 2015 - 05:54:30)

CPU:   Freescale LayerScape LS1021E, Version: 1.0, (0x87081110)

Clock Configuration:

       CPU0(ARMV7):1000 MHz,

       Bus:300  MHz, DDR:800  MHz (1600 MT/s data rate),

Reset Configuration Word (RCW):

       00000000: 0608000a 00000000 00000000 00000000

       00000010: 70000000 00007900 e0025a00 21046000

       00000020: 00000000 00000000 00000000 00038000

       00000030: 00080000 48007340 00000000 00000000

Board: LS1021ATWR

CPLD:  V2.3

PCBA:  V4.0

VBank: 0

I2C:   ready

DRAM:  1 GiB

Using SERDES1 Protocol: 112 (0x70)

Firmware 'Microcode version 0.0.0 for T1040 r1.0' for 1040 V1.0

QE: uploading microcode 'Microcode for T1040 r1.0'

Flash: 128 MiB

MMC:   FSL_SDHC: 0

EEPROM: CRC mismatch (d28e9fc5 != ffffffff)

PCIe1: Root Complex x1 gen1, regs @ 0x3400000

     01:00.0    - 14e4:43a0 - Network controller

PCIe1: Bus 00 - 01

PCIe2: Root Complex no link, regs @ 0x3500000

In:    serial

Out:   serial

Err:   serial

SATA link 0 timeout.

AHCI 0001.0300 1 slots 1 ports ? Gbps 0x1 impl SATA mode

flags: 64bit ncq pm clo only pmp fbss pio slum part ccc

scanning bus for devices...

Found 0 device(s).

Net:   eTSEC2 is in sgmii mode.

eTSEC1 [PRIME], eTSEC2, eTSEC3

Hit any key to stop autoboot:  0

=>

=> sata init

Unknown command 'sata' - try 'help'

Please help me to resolve this issue..

Thank you in advance :smileyhappy:

标签 (1)
标记 (2)
1 解答
7,510 次查看
artsiomstaliaro
Contributor IV

Need to rebuild Linux kernel with:

1. In Kernel menuconfig Device drivers->Serial ATA and Parallel ATA

     [*] SATA Port Multiplier support

     <*> AHCI SATA support

     <*> Freescale 3.0Gbps SATA support

2. In Kernel menuconfig Device drivers->SCSI device support-> <*> SCSI disk support

3. In Kernel menuconfig File systems->

     <*> Second extended fs support
     <*> Ext3 journalling file system support

     Partition Types ->

     [*] Advanced partition selection

     [*] PC BIOS (MSDOS partition tables) support

     Native Language Support ->

     (iso8859-1) Default NLS Option

     <*> Codepage 437 (United States, Canada)

     <*> NLS ISO 8859-1 (Latin 1; Western European Languages)

在原帖中查看解决方案

8 回复数
7,510 次查看
yipingwang
NXP TechSupport
NXP TechSupport

Hello Vignesh R,

Please check whether the following information could help you.

U-Boot 2014.07+ls1+g659b6a2 (Mar 10 2015 - 10:30:21)

CPU:  Freescale LayerScape LS1021E, Version: 1.0, (0x87081110)

Clock Configuration:

      CPU0(ARMV7):1000 MHz,

      Bus:300  MHz, DDR:800  MHz (1600 MT/s data rate),

Reset Configuration Word (RCW):

      00000000: 0608000a 00000000 00000000 00000000

      00000010: 70000000 00007900 e0025a00 21046000

      00000020: 00000000 00000000 00000000 00038000

      00000030: 00080000 48007340 00000000 00000000

Board: LS1021ATWR

CPLD:  V2.3

PCBA:  V4.0

VBank: 0

I2C:  ready

DRAM:  1 GiB

Using SERDES1 Protocol: 112 (0x70)

Firmware 'Microcode version 0.0.0 for T1040 r1.0' for 1040 V1.0

QE: uploading microcode 'Microcode for T1040 r1.0'

Flash: 128 MiB

MMC:  FSL_SDHC: 0

EEPROM: NXID v1

PCIe1: Root Complex no link, regs @ 0x3400000

PCIe2: Root Complex no link, regs @ 0x3500000

In:    serial

Out:  serial

Err:  serial

Target spinup took 0 ms.

AHCI 0001.0300 1 slots 1 ports ? Gbps 0x1 impl SATA mode

flags: 64bit ncq pm clo only pmp fbss pio slum part ccc

scanning bus for devices...

  Device 0: (0:0) Vendor: ATA Prod.: ST3160815AS Rev: 4.AD

            Type: Hard Disk

            Capacity: 152587.8 MB = 149.0 GB (312500000 x 512)

Type: Hard Disk

            Capacity: 152587.8 MB = 149.0 GB (312500000 x 512)

Found 1 device(s).

Net:  eTSEC2 is in sgmii mode.

eTSEC1, eTSEC2 [PRIME], eTSEC3

=>

=> scsi info

SCSI dev. 0:  (0:0) Vendor: ATA Prod.: ST3160815AS Rev: 4.AD

            Type: Hard Disk

            Capacity: 152587.8 MB = 149.0 GB (312500000 x 512)

=> scsi rescan

Reset SCSI

scanning bus for devices...

  Device 0: (0:0) Vendor: ATA Prod.: ST3160815AS Rev: 4.AD

            Type: Hard Disk

            Capacity: 152587.8 MB = 149.0 GB (312500000 x 512)

Found 1 device(s).

=> scsi

scsi - SCSI sub-system

Usage:

scsi reset - reset SCSI controller

scsi info  - show available SCSI devices

scsi scan  - (re-)scan SCSI bus

scsi device [dev] - show or set current device

scsi part [dev] - print partition table of one or all SCSI devices

scsi device [dev] - show or set current device

scsi part [dev] - print partition table of one or all SCSI devices

scsi read addr blk# cnt - read `cnt' blocks starting at block `blk#'

    to memory address `addr'

scsi write addr blk# cnt - write `cnt' blocks starting at block

    `blk#' from memory address `addr'

=> scsi device 0

SCSI device 0:

    Device 0: (0:0) Vendor: ATA Prod.: ST3160815AS Rev: 4.AD

            Type: Hard Disk

            Capacity: 152587.8 MB = 149.0 GB (312500000 x 512)

... is now current device

=> scsi device 0:1

SCSI device 0:

    Device 0: (0:0) Vendor: ATA Prod.: ST3160815AS Rev: 4.AD

            Type: Hard Disk

            Capacity: 152587.8 MB = 149.0 GB (312500000 x 512)

... is now current device

=> scsi part 1

## Unknown partition table

=> scsi part 0

Partition Map for SCSI device 0  --  Partition Type: DOS

Part    Start Sector    Num Sectors    UUID            Type

  1    2048            312497952      a288bb3e-01    83

=> scsi read 81000000 32 10

SCSI read: device 0 block # 50, count 16 ... timeout exit!

16 blocks read: OK


Have a great day,
Yiping

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

7,510 次查看
vigneshr
Contributor III

Hi Yiping,

Ya, I was able to see all those logs in my u-boot, but in kernel i want to access the hard disk. I done dmesg but hard disk is not detected there. How to resolve it ?

Thanks,

0 项奖励
回复
7,511 次查看
artsiomstaliaro
Contributor IV

Need to rebuild Linux kernel with:

1. In Kernel menuconfig Device drivers->Serial ATA and Parallel ATA

     [*] SATA Port Multiplier support

     <*> AHCI SATA support

     <*> Freescale 3.0Gbps SATA support

2. In Kernel menuconfig Device drivers->SCSI device support-> <*> SCSI disk support

3. In Kernel menuconfig File systems->

     <*> Second extended fs support
     <*> Ext3 journalling file system support

     Partition Types ->

     [*] Advanced partition selection

     [*] PC BIOS (MSDOS partition tables) support

     Native Language Support ->

     (iso8859-1) Default NLS Option

     <*> Codepage 437 (United States, Canada)

     <*> NLS ISO 8859-1 (Latin 1; Western European Languages)

7,510 次查看
vigneshr
Contributor III

Hi Art,

Thanks, now I'm able to detect hard disk in kernel. Now can you help me how to add SATA command in the u-boot. I have added SATA command in u-boot by adding some macros in ls1021atwr.h and config_cmd_all.h file from the u-boot source file. But I can able to use only sata command. Not able to use sata init , read, write etc. What could be the reason and solution for this issue.?

0 项奖励
回复
7,510 次查看
artsiomstaliaro
Contributor IV

What should do 'sata' command?

For example, you have FAT on SATA HDD and you need to boot uImage from FAT partition.

So:

setenv sata 'fatload scsi 0:0 81000000 uImage'

7,510 次查看
vigneshr
Contributor III

Okay Art,
Thanks.

0 项奖励
回复
7,510 次查看
artsiomstaliaro
Contributor IV

Hello,

please use "scsi scan" .

0 项奖励
回复
7,510 次查看
vigneshr
Contributor III

Hi Art,


Thanks,

With scsi scan i was able to detect the hard disk in u-boot, but in kernel i was not able to access the disk. what should be done to detect the device in kernel ?

and also please let me know how to add sata command in u-boot ..

0 项奖励
回复