LS1021A

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 
4,569 Views
sukruthrameshba
Contributor III

Hello,

We are starting a new project with the eval board using LS1021A processor.

Can you please provide the demo software (preferably with CAN and Ethernet Driver)?

Note that we are using CodeWarrior platform and it will be helpful if you can provide Code Warrior project file.

Regards,

Sukruth. 

Labels (1)
Tags (1)
0 Kudos
Reply
1 Solution
4,100 Views
Pavel
NXP Employee
NXP Employee

NXP offers SDK Linux BSP for the LS1021a. This BSP supports Ethernet and FlexCAN of the LS1021a.

See documentation for this SDK on the following page:

http://www.nxp.com/products/software-and-tools/run-time-software/linux-sdk/linux-sdk-for-qoriq-proce...

 

Attached file contains drivers from this SDK.

 

NXP offers CodeWarrior for the LS1021a:

http://www.nxp.com/products/software-and-tools/software-development-tools/codewarrior-development-to...


Have a great day,
Pavel Chubakov

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

6 Replies
4,100 Views
sukruthrameshba
Contributor III

Dear Pavel,

We are using a custom made eval board in which we used LS1021A processor and peripherals from other suppliers.

Now We are starting software development for this board, for which we are evaluating Code Warrior IDE.

Can you please provide simple GPIO configuration if available? , to test on our board.

0 Kudos
Reply
4,100 Views
Pavel
NXP Employee
NXP Employee

CodeWarrior contains example for DUART. See Examples in CodeWarrior folder.


Have a great day,
Pavel Chubakov

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply
4,100 Views
sukruthrameshba
Contributor III

Thank you.

I have installed CodeWarrior IDE for LS1021a. 

Can you please provide the example project on this processor?(Preferably with all the basic drivers)

0 Kudos
Reply
4,100 Views
Pavel
NXP Employee
NXP Employee

NXP offers SDK Linux BSP for the LS1021a:

http://www.nxp.com/products/software-and-tools/run-time-software/linux-sdk/linux-sdk-for-qoriq-proce...

 

NXP offers CodeWarrior IDE for ARM LS1021a:

http://www.nxp.com/products/software-and-tools/software-development-tools/codewarrior-development-to...

 

This CodeWarrior provides startup code for the LS1021a.

NXP provides CodeWarrior for Windows and for Linux.


Have a great day,
Pavel Chubakov

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

4,101 Views
Pavel
NXP Employee
NXP Employee

NXP offers SDK Linux BSP for the LS1021a. This BSP supports Ethernet and FlexCAN of the LS1021a.

See documentation for this SDK on the following page:

http://www.nxp.com/products/software-and-tools/run-time-software/linux-sdk/linux-sdk-for-qoriq-proce...

 

Attached file contains drivers from this SDK.

 

NXP offers CodeWarrior for the LS1021a:

http://www.nxp.com/products/software-and-tools/software-development-tools/codewarrior-development-to...


Have a great day,
Pavel Chubakov

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

4,100 Views
sukruthrameshba
Contributor III

Dear Pavel ,

Thank you for your reply.

I had used MPC5668G microcontroller for my earlier project.

We had got the startup code from NXP on Windows platform and compilable on CodeWarrior.

Now we are moving to LS1021A , but we need to reuse the code developed with the above platform.

So Can you please provide the SDK that is similar to MPC5668G?

Regards,

Sukruth.

0 Kudos
Reply