LS1021A v2.0 - microcode version

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LS1021A v2.0 - microcode version

ソリューションへジャンプ
2,786件の閲覧回数
Davisg
Contributor III

Is the following the correct microcode version for the LS1021A v2.0?

CPU:   Freescale LayerScape LS1021, Version: 2.0, (0x87001120)

.

.

.

Firmware 'Microcode version 0.0.1 for LS1021a r1.0' for 1021 V1.0

QE: uploading microcode 'Microcode for LS1021a r1.0' version 0.0.1

ラベル(1)
0 件の賞賛
返信
1 解決策
2,571件の閲覧回数
r8070z
NXP Employee
NXP Employee


Have a great day,


yes, this message shows the correct microcode version for the LS1021A v2.0

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
2,572件の閲覧回数
r8070z
NXP Employee
NXP Employee


Have a great day,


yes, this message shows the correct microcode version for the LS1021A v2.0

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信