LS1021A development that boots from NAND

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LS1021A development that boots from NAND

1,807件の閲覧回数
keestrommel
Contributor IV

Does someone know whether a LS1021A development board exists that boots or can boot from NAND flash?

ラベル(1)
0 件の賞賛
返信
1 返信

1,570件の閲覧回数
alexander_yakov
NXP Employee
NXP Employee

According to LS1021A product page, currently we offer two development boards based on LS1021A device - TWR and IoT.

For both these boards - there is no NAND flash on board schematic, so booting from NAND flash is not supported.


Have a great day,
Alexander

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信