LS1021A and PCIe

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LS1021A and PCIe

3,270件の閲覧回数
artsiomstaliaro
Contributor IV

Hello,

im working with PCIe from baremetal application where no MMU.

Is it possible access to PCIe memory (0x40_0000_0000) with qDMA? Is possible to read PCIe CFG with qDMA?

Maybe exist another way for reading data from this memory without MMU?

ラベル(1)
タグ(3)
0 件の賞賛
返信
2 返答(返信)

2,676件の閲覧回数
r8070z
NXP Employee
NXP Employee


Have a great day,

It is possible access to PCIe memory with qDMA but SMMU and translation windows should be configured properly.

0 件の賞賛
返信

2,676件の閲覧回数
artsiomstaliaro
Contributor IV

Thank you for answer.

Memory translation is not possible with SMMU (errata)

What i can do: to configure ATU in PCIe and set correct SMMU S2CR configuration.

Can you describe more about SMMU configuration?

My current algorithm is:

1. Setup SMMU2 NSCR register, where clears "Client Port Disable" bit and clears "Memory Type Configuration"  bit to set default memory attributes.

2. Setup SMMU2 SMR Stream ID number for PCIe

3. Setup SMMU2 S2CR register with Write&Read allocate, Bypass type, Cacheable memory attribute.

4. Setup PCIe1: setup link and configure iATU. (If MMU translation is enable, so I able to read PCIe WIFI card CFG0 data from mapped address).

5. Setup qDMA legacy channel in qDMA manager to copy 256 bytes from PCIe1 memory (0x4000000000) to DDR3 (0x80300000).

6. Check DLSR register in qDMA manager: DLSR_CB is set constantly. So copy cannot be completed.

0 件の賞賛
返信