LS1021A SEC CRCA Dynamic Custom Mode

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

LS1021A SEC CRCA Dynamic Custom Mode

跳至解决方案
3,594 次查看
Xi-nanWang
Contributor II

LS1021A, I use SEC for hardware CRC calculation, I can only run the STANDARD IEEE and IETF mode correctly, when it comes to Dynamic CUSTOM mode, the hardware will generate all ZERO results. The register configuration are the same except the mode selection AAI and Key Register. Did I miss any critical register bits? Or which registers should I consider to use CRCA dynamic custom mode?

标签 (2)
标记 (3)
0 项奖励
回复
1 解答
3,444 次查看
bpe
NXP Employee
NXP Employee

Generating CRC with custom polynomials require a Job Descriptor that
is not in the standard JD library. Customers requiring custom crypto
operation descriptors are advised to request them through NXP
paid Professional Services:

Commercial Support and Engineering Services | NXP 

Regards,

Platon

在原帖中查看解决方案

4 回复数
3,445 次查看
bpe
NXP Employee
NXP Employee

Generating CRC with custom polynomials require a Job Descriptor that
is not in the standard JD library. Customers requiring custom crypto
operation descriptors are advised to request them through NXP
paid Professional Services:

Commercial Support and Engineering Services | NXP 

Regards,

Platon

3,444 次查看
Xi-nanWang
Contributor II

Resently I have encountered some problems when using SEC to calculate MD5. Since the source data size is too too big, i hope to splite it into chunks and calculate in times. Which registers should i concerned about and how to config? or does it need some sort of paid services again? 

0 项奖励
回复
3,444 次查看
Xi-nanWang
Contributor II

Thx a lot.

0 项奖励
回复
3,444 次查看
Xi-nanWang
Contributor II

Nobody has any clue? Or my statement is too vague? Any answer would help.

0 项奖励
回复